Output voltage is higher than specified - why?

Some converters need some load for an effective function of the regulation.
It is specified under “Minimum Load”. If the load is below that value the output voltage can be some 100mV up to a view Volts higher than specified.  Operation in this range does not damage the converter but might have a bad impact in your application.
New converters are designed for no minimum load requirement. But even if you measure such a converter at no load operation with a highly resistive probe, it might show a higher voltage or ripple than specified.

Operating temperature range - What does it mean?

The operating temperature range of a device is meant as the ambient temperature you would theoretically measure at the device under the assumption that the device does not produce any heat by itself.
That means, it is the temperature inside the application including every heat source around the device.
Be aware, that the operating temperature of the application is not the same as the operating temperature range of the device inside the application.

AC input voltage range on the label is different than spezified on datasheet - Why?

The wider input range on datasheet specifies the range the product is designed for. The smaller range on the label conforms to the mains it can be used for, which is an issue for certification and it considers that mains have a tolerance of ±10%. If a Power Supply is certified for mains voltage from 100 to 240 VAC the input circuit has to be designed for 90 to 264 VAC.

Protection class I or II - What is the difference?

In a Class II appliance, the user is protected by at least two layers of insulation (double or reinforced) between the current carrying parts and any metal accessible to the user.
In Class I appliances, the protection is provided by a combination of basic insulation and the use of protective earth. These appliances must have their chassis connected to electrical earth by an earth conductor (green/yellow)

Serial connection of two converters - Is this possible?

Although it is possible to connect two AC/DC or DC/DC converters in series on output side (including freewheeling diodes), we do not generally recommend it, because a technical or safety issue might occur if not carefully tested in customer’s application and in accordance to the applicable safety regulations (e.g. SELV requirements).
Generally, it cannot be assumed, that any interconnection of two converters operate in each application condition as they would in a single operation (e.g. start-up behaviour, regulation, ripple & noise, …). Our datasheet specifies the characteristic of a single converter under nominal values and full load but not in an interconnection.

Parallel connection of two converters - Can it be done?

Although it is possible to connect two AC/DC or DC/DC converters in parallel on output side (including decoupling diodes), we do not generally recommend it, because the load sharing is unknown.  For redundant operation, it might be a possible approach, but it has to be ensured in customer’s application, that it works as it is intended for. 
Generally, it cannot be assumed, that any interconnection of two converters operate in each application condition as they would in a single operation (e.g. start-up behaviour, regulation, ripple & noise, …). Our datasheet specifies the characteristic of a single converter under nominal values and full load but not in an interconnection.

Safety report availability – Can you send the safety report to me?

Test reports are confidential and will not be provided to customers or distributors. If you or your customer will certify the end-application (containing Traco Power products), you can name us the notified body (accredited test labs only) including the responsible engineer at the lab and the project (name or number and the required standard). After that, we will send the test report to the test lab directly.

EN45545-2 - What does it stand for?

The identified flammable materials are tested according to requirement set R24 of 45545-2 and fulfil the oxygen content requirements of hazard levels HL1, HL2 and HL3. The remaining combustible mass of each product in the mentioned series is below 100g and can be excluded from further EN 45545-2 considerations in the final interior or exterior application while observing the grouping rules. A manufacturer declaration is available on request.

Product status - What does it mean?